:LTESt:MEASure:EYE:LOCation:LLIMit
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:LLIMit
insead.
Command Syntax
:LTESt:MEASure:EYE:LOCation{1:32}:LLIMit <limit>
<limit> is a double.
Query Syntax
:LTESt:MEASure:EYE:LOCation{1:32}:LLIMit?
Description
Defines the lower limit for an eye measurement limit test in Eye/Mask mode. For example, if you chose to measure eye width and want the smallest acceptable variation to be 90 ps ±5 ps, set the lower limit to 85 ps and the upper limit to 95 ps, and then set the limit test to fail when the signal is outside the specified limit.
The eye measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:EYE:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off. Use the following sibling commands to configure the measurement: