Jitter Mode Measurements

Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA

In Jitter mode, measurements are displayed in the dedicated results panels and are organized under the SCPI nodes shown in the following table.

Jitter mode supports NRZ and PAM4 formatted waveforms. Jitter mode does not support PAM6 and PAM8 waveforms.

Measurements versus SCPI Nodes
Waveform Format Measurement Type Results Panel SCPI Node
NRZ Jitter Jiiter :MEAS:JITTer
Interference Amplitude :MEAS:AMPLitude
Phase-Only Jitter Timing Jitter :MEAS:JITTer:POJitter
PAM4 Jitter Eye :MEAS:PEYE
Interference Level :MEAS:PLEVel
12-Edge Output Jitter Output Jitter :MEAS:JITTer:OJITter
Phase-Only Jitter Timing Jitter :MEAS:JITTer:POJitter

Deprecated Commands