Oscilloscope Mode Measurements
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
All Oscilloscope Mode measurements are displayed in the Results panel. This includes Time, Amplitude, PAM, and User measurements. NRZ time and amplitude Measurements are optimized for NRZ signals but, as noted, may work with PAM4 signals. PAM4 measurements are optimized for PAM4 signals. If used with an NRZ signal, the low and high level results are reported as levels 0 and 3 while the level 1 and 2 results are not valid. To define measurement regions over which the measurements are made, use the commands in the :MEAS:REGions SCPI command node.
:MEASure Subsystem
Deprecated Scope Commands
Scope Mode Commands Groups
User Measurements (Scope) Commands
- Scope Mode
- User Measurements
- :MEASure:OSCilloscope:USER
- :MEASure:OSCilloscope:USER:ABBReviation?
- :MEASure:OSCilloscope:USER:CFILe
- :MEASure:OSCilloscope:USER:CFILe:CLEar
- :MEASure:OSCilloscope:USER:CFILe:RELoad
- :MEASure:OSCilloscope:USER:CFLoaded?
- :MEASure:OSCilloscope:USER:COMMents?
- :MEASure:OSCilloscope:USER:LOCation?
- :MEASure:OSCilloscope:USER:LSTatus?
- :MEASure:OSCilloscope:USER:LSTatus:REASon?
- :MEASure:OSCilloscope:USER:NAME?
- :MEASure:OSCilloscope:USER:REGion
- :MEASure:OSCilloscope:USER:SOURce{1:2}
- :MEASure:OSCilloscope:USER:STATus?
- :MEASure:OSCilloscope:USER:STATus:DETails?
- :MEASure:OSCilloscope:USER:STATus:REASon?
PAM4 Amplitude Commands
NRZ Time Commands
- Scope Mode
- :MEASure:OSCilloscope:DELTatime
- :MEASure:OSCilloscope:DUTYcycle
- :MEASure:OSCilloscope:FALLtime
- :MEASure:OSCilloscope:FREQuency
- :MEASure:OSCilloscope:JITTer
- :MEASure:OSCilloscope:NWIDth
- :MEASure:OSCilloscope:PERiod
- :MEASure:OSCilloscope:PHASe
- :MEASure:OSCilloscope:PWIDth
- :MEASure:OSCilloscope:RISetime
- :MEASure:OSCilloscope:TEDGe
- :MEASure:OSCilloscope:TMAXimum
- :MEASure:OSCilloscope:TMINimum
- :MEASure:OSCilloscope:TVOLt
NRZ Amplitude Commands
- Scope Mode
- :MEASure:OSCilloscope:APOWer
- :MEASure:OSCilloscope:OMAmplitude
- :MEASure:OSCilloscope:OVERshoot
- :MEASure:OSCilloscope:PPHRatio
- :MEASure:OSCilloscope:PREShoot
- :MEASure:OSCilloscope:VAMPlitude
- :MEASure:OSCilloscope:VAVerage
- :MEASure:OSCilloscope:VBASe
- :MEASure:OSCilloscope:VLOWer
- :MEASure:OSCilloscope:VMAXimum
- :MEASure:OSCilloscope:VMIDdle
- :MEASure:OSCilloscope:VMINimum
- :MEASure:OSCilloscope:VPP
- :MEASure:OSCilloscope:VRMS
- :MEASure:OSCilloscope:VTIMe
- :MEASure:OSCilloscope:VTOP
- :MEASure:OSCilloscope:VUPPer