TDR/TDT Mode Measurements
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
In TDR Mode, the SCPI commands all measurements are located in the :MEAS:TDR SCPI command node. To define measurement regions over which the measurments are made, use the commands in the :MEAS:REGions SCPI command node. Use TDR user measurement commands to create custom user-defined measurements that are based on Matlab or Python scripts. When the measurement is created, a button is automatically placed on TDR/TDT Mode's User toolbar.
User Opterators and User Defined Measurements are provided with the Research and Developement Package. These features are also part of the legacy N1010A-201 Advanced Waveform Analysis license.
TDR measurements require FlexDCA revision A.04.00 and above.