:MEASure:EYE:COMPlete
Command Syntax
:MEASure:EYE:COMPlete <peak hits>
<peak hits> is an integer.
Query Syntax
:MEASure:EYE:COMPlete?
Returns the current setting for color grade completion.
Description
Sets the peak numbers-of-hits required in the color grade database before a color grade measurement is made on the data. This completion criteria is also by auto skew. So, if auto skew fails to make the symbol rate measurement or the time of the crossing points (both needed to compute the skew), it may be necessary to increase the color grade completion criterion. Increasing the value increases the time for auto skew to complete, allowing it to collect more data points before executing the symbol rate and crossing time measurements
A color grade measurement query will return 9.99999E+37 until the measurement is complete.
Requires FlexDCA revision A.03.00 and above.