:SYSTem:SOFTware:FEATures:AFRemoval:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-SNT
Query Syntax
:SYSTem:SOFTware:FEATures:AFRemoval:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the Automatic Fixture Removel feature is enabled and returns "0" if the feature is not enabled. To enable this feature, purchase the Signal Integrity Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:AFRemoval:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.