:SYSTem:SOFTware:FEATures:AWANalysis:EQUalizers:VERSion?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Query Syntax
:SYSTem:SOFTware:FEATures:AWANalysis:EQUalizers:VERSion?
Query Response
"<version number>"
Description
Returns the version of the Advanced Waveform Analysis Equalizers feature, if it is enabled. For example, "1.000"
. To determine is the feature is installed, use the :SYSTem:SOFTware:FEATures:AWANalysis:EQUalizers:ENABled?
query.
If the feature license is not installed, error -400,"Query error;License is not installed" is generated.
Requires FlexDCA revision A.05.80 and above.