:SYSTem:SOFTware:FEATures:AWANalysis:UDOPerations:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
L-SNT
Query Syntax
:SYSTem:SOFTware:FEATures:AWANalysis:UDOPerations:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the Advanced Waveform Analysis User Operators feature is enabled and returns "0" if the feature is not enabled. Advanced Waveform Analysis Equalizers provides the following operators:
- User Operators
- User Defined Measurements
To enable this feature, purchase the Research and Development Package or Signal Integrity Package license. Advanced Waveform Analysis User Operators feature is also available with license 201.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:AWANalysis:UDOPerations:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.