:SYSTem:SOFTware:FEATures:FEYE:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Query Syntax
:SYSTem:SOFTware:FEATures:FEYE:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the FlexEye Independent Eye Acquisition and Analysis feature is enabled and returns "0" if the feature is not enabled. The FlexEye Independent Eye Acquisition and Analysis feature greatly reduces Eye mode measurement test times in computer-controlled environments. The FlexEye feature runs measurements asynchronously by turning selected input channels into independent FlexDCA sampling oscilloscopes known as sessions.
To enable this feature, purchase the Research and Development Package or Manufacturing Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:FEYE:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.