:SYSTem:SOFTware:FEATures:FLEX:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
L-SNT
L-MFG
Query Syntax
:SYSTem:SOFTware:FEATures:FLEX:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the FLEX feature is enabled and returns "0" if the feature is not enabled. FLEX enables the N1010A FlexDCA on a PC to control FlexDCA on an 86100D or to control a DCA-M series module. To enable this feature, purchase FLEX Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:FLEX:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.