:SYSTem:SOFTware:FEATures:ISIM:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
Query Syntax
:SYSTem:SOFTware:FEATures:ISIM:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the InfiniiSim-DCA Waveform Transformation Toolset feature is enabled and returns "0" if the feature is not enabled. InfiniiSim-DCA Waveform Transformation Toolset provide de-embedding and embedding capability to the FlexDCA application. Once the license is installed, access this feature from the Waveform Signal Processing tool. Click Measure > Waveform Signal Processing.
To enable this feature, purchase the Research and Development Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:ISIM:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.