:SYSTem:SOFTware:FEATures:JITTer:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
Query Syntax
:SYSTem:SOFTware:FEATures:JITTer:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the Enhanced Jitter Analysis feature is enabled and returns "0" if the feature is not enabled. Enhanced Jitter Analysis activates Jitter Mode to provide jitter analysis tools. Once installed, you can activate Jitter mode by the Jitter Mode button. Results are provided in both tables and graphs. You can extend Jitter Mode into the amplitude domain by adding the Advanced Amplitude Analysis/RIN/Q-factor license 300.
To enable this feature, purchase the Research and Development Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:JITTer:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.