:SYSTem:SOFTware:FEATures:MEASure:TDEC:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
L-MFG
Query Syntax
:SYSTem:SOFTware:FEATures:MEASure:TDEC:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the TDEC Measurement feature is enabled and returns "0" if the feature is not enabled. TDEC Measurement is and Eye mode measurement on NRZ waveforms.
To enable this feature, purchase the Research and Development Package or Manufacturing Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:MEASure:TDEC:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.