:SYSTem:SOFTware:FEATures:TDCQ:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Applicable Licenses:
L-RND
L-SNT
L-MFG
Query Syntax
:SYSTem:SOFTware:FEATures:TDCQ:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the TDECQ Transmitter and Dispersion Eye Closure for PAM4 feature is enabled and returns "0" if the feature is not enabled. This feature provides Transmitter and Dispersion Eye Closure for PAM4 measurements for the quality of an optical transmitter with its optical link. To enable this feature, purchase the Research and Development Package , Manufacturing Package , or Signal Integrity Package license.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:TDCQ:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.