:SYSTem:SOFTware:FEATures:UDIMport:ENABled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
L-SNT
L-MFG
Query Syntax
:SYSTem:SOFTware:FEATures:UDIMport:ENABled?
Query Response
{1 | 0}
Description
Returns "1" if the Unrestricted Import feature is enabled and returns "0" if the feature is not enabled. This feature is part of the Enhanced Jitter Analysis license 200 provides which gives FlexDCA unrestricted capability to import data files into FlexDCA's waveform memory, color grade-gray scale memory, and simulated module's source waveform type.
To return the version of the license, use the :SYSTem:SOFTware:FEATures:UDIMport:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.