:SYSTem:SOFTware:LICenses:SFEature:AFRemoval:INSTalled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Query Syntax
:SYSTem:SOFTware:LICenses:SFEature:AFRemoval:INSTalled?
Query Response
{1 | 0}
Description
Returns "1" if the Automatic Fixture Removal software feature license BFP is installed and returns "0" if the license is not installed. To return the name of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:FEATure?
query. To return the version number of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.