:SYSTem:SOFTware:LICenses:SFEature:FLEX:INSTalled?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Query Syntax
:SYSTem:SOFTware:LICenses:SFEature:FLEX:INSTalled?
Query Response
{1 | 0}
Description
Returns "1" if the FlexDCA software feature license is installed and returns "0" if the license is not installed. To return the name of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:FEATure?
query. To return the version number of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.