:SYSTem:SOFTware:LICenses:SFEature:ISIM:FEATure?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Query Syntax
:SYSTem:SOFTware:LICenses:SFEature:ISIM:FEATure?
Query Response
"InfiniiSim-DCA"
Description
Returns a string that identifies the name of the InfiniiSim-DCA Waveform Transformation Toolset software feature license SIM . To determine if the license is installed, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:INSTalled?
query. To return the version number of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:VERSion?
query.
Requires FlexDCA revision A.05.80 and above.