:SYSTem:SOFTware:LICenses:SFEature:ISIM:VERSion?
Removed command for revision A.06.00 and above. This command is no longer available.
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Query Syntax
:SYSTem:SOFTware:LICenses:SFEature:ISIM:VERSion?
Description
Returns the version number of the InfiniiSim-DCA Waveform Transformation Toolset software feature license SIM . For example, "1.000"
. Returns an empty string if the license is not installed. To determine if the temporary license is installed, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:INSTalled?
query. To return the name of the license, use the :SYSTem:SOFTware:LICenses:SFEature:AEYE:FEATure?
query.
If the feature license is not installed, error -400,"Query error;License is not installed" is generated.
Requires FlexDCA revision A.05.80 and above.