Specify pattern for equalizers and jitter mode

Flex Apps:
FlexDCA

The F-SKP feature provides the ability to specify the pattern for jitter mode and for the following waveform signal processing equalizers:

  • Jitter Mode setup
  • Decision Feedback Equalizer
  • Linear Feed Forward Equalizer
  • TDECQ Reference Equalizer

You can specify a known pattern (NRZ or PAM4) or load a specific pattern file.