SNDR
Signal-to-Noise-and-Distortions Feature
Enables the Signal-to-Noise-and-Distortion Ratio (SNDR) measurement and supporting measurements P-Signal, Sigma-E, and Sigma-N. For the output signal of a transmitter, the SNDR measurement compares a calculated ideal signal (linear pulse fit) to the measured signal. You can access the SNDR measurement on Jitter Mode's Meas toolbar. The measurement results are displayed on the Level results table. To remotely run the measurement, use the :MEASure:PLEVel:SNDRatio command).