SFF-8431 Module Measurement Suite
The SFF-8431 Module Measurement Suite license enables the use of the Keysight N1014A-2FP Compliance and Debug Application. This application installs on a PC or DCA-X and measures your high speed serial module or IC to all required transmit parameters in the SFF-8431 Specifications. Take advantage of the industry’s lowest intrinsic jitter from the 86108B Precision Waveform Analyzer.
If you plan to run all of the N1014A tests, you will need the additional SFF-8431 Host Measurement Suite license (N1014A-HST).
To enable the use of the U3020AS26 switching test set with this compliance and debug application, purchase the SFF-8431 Measurement Suite Switch Control license.