FlexDCA Remote Access
The FLEX feature allows N1010A FlexDCA running on a PC to make a live connection to FlexDCA (A.05.30 or later) running on an N1000A.
It is required that the feature license be installed on the PC (not on the DCA-X mainframe) in order to enable this feature. Once the live connection is made, all DCA software options installed on the DCA-X mainframe will be recognized by FlexDCA running on the PC. Subscription-based compliance application licenses installed on the DCA-X mainframe will not be recognized.
This feature is included in these package licenses: