Firewall
If you cannot establish remote connection to the N1000A, the instrument's Windows Firewall may be blocking access to ports 4880, 5024-5025. This procedure shows you how to enable these ports. These settings allow control of the instrument over SICL/LAN and allow the Keysight Connection Expert to locate the instrument.
- Minimize the FlexDCA application to view the Windows desktop.
- In the Windows Start, click the Search field and type "Windows Firewall". When the search completes, select Windows Firewall with Advanced Security.
- In the Windows Firewall with Advanced Security application, select Inbound Rules in the left pane. Then, in the right pane, click New Rule.
- In the New Inbound Rule Wizard, select Port and then Next. Select the Specific local ports field and enter: 4880, 5024-5025. Then, click Next.
- In the Action panel, select Allow the connection. Then, click Next.
- In the Profile panel, select Domain, Private, and Public. Then, click Next.
- In the Name panel, name your rule and then click Finish.