SCPI Server Setup

Use the SCPI Server Setup dialog to setup the interface used for the following tasks:

  • Configure FlexDCA to be controlled via remote programming commands.
  • Connecting N1010A FlexDCA on a PC to FlexDCA on a N1000A instrument.

If you have problems connecting to a N1000A, the Window's Firewall may be blocking the appropriate ports which must be enabled for 4880, 5024-5025.

When you click a Setup button, one of the interface dialogs described later in this topic opens to allow you to configure the selected interface. After entering the server settings, be sure to select Enable. The dialog lists the addresses that you use to identify the LAN address between your program and FlexDCA. For example, the VISA address for the HiSLIP interface is easy to locate and is used

  1. From the dialog, write down the complete listed VISA Address for HiSLIP. As an alternative, you can highlight the string using the mouse cursor and press Ctrl-C to copy it to the clipboard for later use. In the above picture, the string for HiSLIP would be:
  2. TCPIP0::2UA2421081::hislip0,4880::INSTR
  3. Or, you could substitute the IP address as shown here:
  4. TCPIP0::141.121.89.103::hislip0,4880::INSTR
  5. If your program is running on the same PC or N1000A as FlexDCA, you can simplify this string by substituting localhost for the computer name. For example, you would modify the above VISA address to be the following string:
  6. TCPIP0::localhost::hislip0,4880::INSTR
  7. Close the dialog.

GPIB Interface

GPIB is standard on an N1000A. Enter the IEEE-488.2 GPIB (General Purpose Interface Bus) address.

VXI-11 Interface

VXI-11 is a standard I/O protocol used by a VISA (Virtual Instrument Software Architecture) library. Enter the device index and bus address. This interface that is compatible with FlexDCA, FlexPLL, FlexOTO Hardware Diagram, and FlexOTO Stations.

USB Interface

The USB interface is available on the N1000A DCA-X. To form a USB address, requires that you enter the following address fields SCPI Server Setup dialog.

<USB_vendor_identification_number> <USB_product_identification_number> <USB_serial_number:>

USB Identification Numbers
Identification Number
Keysight USB vendor 0x2A8D
N1000A USB product 0x7B01

For an N1000A, the VISA Address would be similar to the following string for an instrument serial number of US57331234.:

USB0::0x2a8d::0x7b01::US57331234::0::INSTR

The only option in the setup dialog is to enable or disable the USB server.

Telnet Interface

Telnet is a standard network protocol. Enter the port on the PC used for network communication. This interface is compatible with FlexDCA, FlexPLL, FlexOTO Hardware Diagram, and FlexOTO Stations.

Starting with FlexDCA revision A.07.90 the Telnet Interface is disabled upon a Factory preset.

Sockets Interface

Enter the PC port used for the sockets interface. This interface that is compatible with FlexDCA, FlexPLL, FlexOTO Hardware Diagram, and FlexOTO Stations.

HiSLIP Interface

The HiSLIP (High-Speed LAN Instrument Protocol) interface facilitates TCP-based instrument control. Enter the device index and PC port used for network communication. This interface that is compatible with FlexDCA, FlexPLL, FlexOTO Hardware Diagram, and FlexOTO Stations. This is also the only interface that is compatible with FlexDCA's FlexEye Independent Eye Acquisition and Analysis.