:CALibrate:MODule:CRECovery
Flex Apps:
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:MODule:CRECovery {ENABled | DISabled | PARTial}, "<DCA-M-name>"
Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".
Query Syntax
:CALibrate:MODule:CRECovery? "<DCA-M-name>"
Description
Enables or disables the clock recovery calibration on the indicated module. Clock recovery is available for N1077A, N1078A, N1092A-CDR, and N1092B-CDR modules. If clock recovery is disabled, the module's vertical calibrations will also be disabled.
- ENABled
-
Selects all clock recovery calibrations for the module to be performed. - DISabled
-
Prevents all clock recovery calibrations for the module from being performed. - PARTial
-
Indicates that some clock recovery calibrations are enabled and some are disabled.
To start the calibration, use the :CALibrate:MODule:STARt command.
Example Command
:CALibrate:MODule:CRECovery ENABled, "N1092A-US12341678"