:CALibrate:MODule:CRECovery:STATus?
Flex Apps:
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CALibrate:MODule:CRECovery:STATus? "<DCA-M-name>"'
Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".
Description
Queries the clock recovery calibration status of a DCA-M module. One of the following response strings is returned:
- "CALIBRATED"
- The clock recovery capability does not require a calibration.
- "UNCALIBRATED"
- The module capability requires a calibration.
Use the following child queries to return details about the current calibration.
| Status String | Query to Send |
|---|---|
| CALIBRATED or UNCALIBRATED |
:CALibrate:MODule:STATus?
:CALibrate:MODule:CRECovery:STATus?
|
| Time of last calibration, time change since last calibration, and temperature change since last calibration |
:CALibrate:MODule:STATus:DETails?
:CALibrate:MODule:CRECovery:STATus:DETails?
|
| Change in temperature | :CALibrate:MODule:STATus:DTEMperature?
:CALibrate:MODule:CRECovery:STATus:DTEMperature?
|
| Change in Time | :CALibrate:MODule:STATus:TIME?
:CALibrate:MODule:CRECovery:STATus:TIME?
|
Requires FlexDCA revision A.07.60 and above for FlexOTO.