:CALibrate:MODule:VERTical:STATus:DETails?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CALibrate:MODule:VERTical:STATus:DETails? "<DCA-M-name>" ["<input-channel>"]
Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".
Optional parameter <input-channel> is a single DCA-M input channel (A, B, C, or D depending on N1092 model). If this parameter is missing, the status will be for the overall vertical calibration.
Description
Queries details concerning the vertical calibration status of a N109x-series DCA-M module's optical channel. The optional input channel is identified by a single channel letter (for example, A, B, C, or D) and does not include a module slot number.
Example Command
:CALibrate:MODule:VERTical:STATus:DETails? "N1092A-US12341678", "A"
Example Response
"Elapsed cal time has exceeded 7 days, Time of last Calibration: 01/24/2023 10:30:19, Elapsed Calibration Time: 21 days, Temperature Change: 0.25degreesC"