:CALibrate:MODule:VERTical:STATus:DTEMperature?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CALibrate:MODule:VERTical:STATus:DTEMperature? "<DCA-M-name>" ["<input-channel>"]
Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".
Optional parameter <input-channel> is a single DCA-M input channel (A, B, C, or D depending on N1092 model). If this parameter is missing, the status will be for the overall vertical calibration.
Description
Queries the change in temperature (°C) status since the last vertical calibration of a N109x-series DCA-M module or module's optical channel. The optional targeted channel is identified by a single channel letter (for example, A, B, C, or D) and does not include a module slot number.
Example Command
:CALibrate:MODule:VERTical:STATus:DETails:DTEMperature? "N1092A-US12341678" "A"
Example Response
2.5E-01