:CONFigure:MODule:ALL?

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Query Syntax

:CONFigure:MODule:ALL?

Query Response

"<model number-serial number>","<model number-serial number>",...

Description

Returns a string of all DCA-M modules that have been recognized by FlexOTO. The string includes all DCA-M modules shown on the Detected DCA-M Modules palette and includes DCA-Ms placed on the Hardware Diagram. Each name is enclosed in double-quote characters and comma-separated. For example:

"N1078A-US78000001","N1092D-US92000001","N1078A-US78000001","N1092D-US92000001","N1092B-US92000001","N1092B-US92000001",...

The following table lists the supported DCA-M modules.

Recognized DCA-M Modules
DCA-M Module Number of
Optical
Channels
Clock Recovery Required Options Connection
Peripheral
Data In Data Out Clock In Clock Out
Oscilloscope Modules
N1092E 2 ● PLK, IRC, 30A/40A USB1
N1092D 4 ● PLK, IRC, 30A/40A USB1
N1092C 1 ● PLK, IRC, 30A/40A USB1
N1092B 2 ● ●2 PLK, IRC, CDR, 30A/40A USB1
N1092A 1 ● ●2 PLK, IRC, CDR, 30A/40A USB1
Clock Recovery Modules
N1078A ● ● ● S50 or SXT3 USB1
N1077B ● ● ● SMM or SXT3 USB1

Supports automatic detection via USB by FlexOTO.

Options CDR and 40A required.

An N1077B-SXT or N1078A-SXT requires an external optical splitter to provide an optical data to an input channel of the N109x-series DCA-M oscilloscope.

Python Example

This simple example, returns from FlexOTO the name of every valid DCA-M module that is recognized. The output also indicates if the module is installed on the Hardware Diagram.

Copy
id-modules.py
import pyvisa as visa
rm = visa.ResourceManager(r'C:\WINDOWS\system32\visa64.dll')
FlexOTO = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR')
FlexOTO.timeout = 5000  # Set connection timeout to 5s
FlexOTO.read_termination = '\n'
FlexOTO.write_termination = '\n'
modules = FlexOTO.query(':CONFigure:MODule:ALL?')
modules = modules.split(',')
print(str(len(modules)) + ' Modules Detected by FlexOTO:')
for module in modules:
    if int(FlexOTO.query(':CONFigure:MODule:ACTive? ' + module)):
        print('\t' + module + ' is installed on Hardware Diagram.')
    else:
        print('\t' + module + ' detected but not placed on Hardware Diagram.')
FlexOTO.write(':SYSTem:GTLocal')
FlexOTO.close()

The output from this script would look similar to this:

6 Modules Detected by FlexOTO:
	N1078A-US78000001 is installed on Hardware Diagram.
	N1078A-US78000002 detected but not placed on Hardware Diagram.
	N1092B-US92000003 detected but not placed on Hardware Diagram.
	N1092B-US92000004 detected but not placed on Hardware Diagram.
	N1092D-US92000001 is installed on Hardware Diagram.
	N1092D-US92000002 detected but not placed on Hardware Diagram.