:CONFigure:MODule:PCRecovery?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CONFigure:MODule:PCRecovery? "<DCA-M-module-name>"
Where <DCA-M-module-name> is a string name that identifies the DCA-M module on the Hardware Diagram.
Query Response
{ON | OFF}
Description
Queries a DCA-M module to discover if the module has clock recovery capability. One of the following tokens can be returned:
OFF- The selected Module does not support clock recovery.
ON- The selected Module does support clock recovery. The module could be an N107x-series clock recovery module or an N109x-series oscilloscope module. You can check the type of module using the
:CONFigure:MODule:DEVice?query.
If a module is not installed (active), the :CONFigure:MODule:PCRecovery? query will still indicate whether the module includes clock recovery.