:CONFigure:MODule:ACTive
Command Syntax
:CONFigure:MODule:ACTive "<DCA-M-module-name>", {ON | OFF}
Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram.
Query Syntax
:CONFigure:MODule:ACTive? "<DCA-M-module-name>"
Query Response
{0 | 1}
Description
Installs or removes a DCA-M module on the Hardware Diagram. You cannot give a module a custom name as you can with Demultiplexers, Impairments, and Instruments. FlexOTO default names for DCA-M modules must be used which are in the form of <model number>-<serial number>. For example, "N1092B-US12345678".
The second command argument can be one of the following tokens:
ON- Installs the selected Module in the Hardware Diagram.
OFF- Uninstalls selected Module from the Hardware Diagram. When sending a query, a returned
OFFindicates that the module is not installed on the Hardware Diagram. If the DCA-M name is not recognized or not supported, an error –224, Illegal parameter vaue;Unknown device name is reported.
When FlexOTO starts, FlexOTO automatically detects all recognized DCA-M modules that are connected. Up to eight modules can be detected. To connect any DCA-M module ports to Switch ports or to another DCA-M module's ports, use the :CONFigure:PORT:CONNect command.
To check the calibration status of a DCA-M module, use the following queries:
To return comma-delimited string of all detected modules, use the :CONFigure:MODule:ALL? query.