:DISK:SETup:RECall
Command Syntax
:DISK:SETup:RECall "filename"
Description
Loads a state setup file into FlexOTO. Use the :DISK:SETup:SAVe command to save a state setup file. Setup files use the .setx file extension and by default are saved in the %USER_DATA_DIR%\Setups folder.
C:\Users\user\Documents\Keysight\FlexOTO\Setups
The hardware (extended module) configuration settings are always saved with a FlexOTO Hardware Diagram state file. When opening an state setup file, use the :SETup:RECall:HCONfig command to select whether to import the extended module configuration settings.
The contents of the setup file for FlexOTO Hardware Diagram is different than a setup file for FlexOTO Stations. When recalling a Setup file, you can only recall Hardware Diagram Setup files into FlexOTO Hardware Diagram and Station Setup files into FlexOTO Stations. Otherwise, error 122 occurs. As a result, if you want to save the setup information of both the Hardware Diagram and all Test Programs, save a Setup file for FlexOTO Hardware Diagram and a Setup file for each FlexOTO Station. When saving a Setup file it is recommended that you append the string "Hardware Diagram" or "Stations#" to the file name to help in identifying the type of Setup file.