:DISK:SETup:RECall:HCONfig
Command Syntax
:DISK:SETup:RECall:HCONfig {ON | OFF}
Query Syntax
:DISK:SETup:RECall:HCONfig?
Description
Enables (ON) or disables (OFF) the loading of extended module configurations when a FlexOTO setup file is opened an using the :DISK:SETup:RECall command. Extended module configurations are always saved with a setup file.
The contents of the setup file for FlexOTO Hardware Diagram is different that a setup file for FlexOTO Stations. When recalling a Setup file, you can only recall Hardware Diagram Setup files into FlexOTO Hardware Diagram and Station Setup files into FlexOTO Stations. Otherwise, error 122 occurs. As a result, if you want to save the setup information of both the Hardware Diagram and all Test Programs, save a Setup file for FlexOTO Hardware Diagram and a Setup file for each FlexOTO Station. When saving a Setup file it is recommended that you append the string "Hardware Diagram" or "Stations#" to the file name to help in identifying the type of Setup file.