:DISK Subsystem

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Location of FlexOTO User Files

Use the :DISK subsystem commands to:

  • Save measurement results into a zip file,
  • Save and recall FlexOTO Hardware Diagram and Station setup files, and to
  • Save screen images.

The Location of FlexOTO User Files picture in this topic shows the FlexOTO folder (with subfolders) for saving files from either a dialog or over SCPI. These folders are the default location for saving specific types of files. Setup files can save time when switching between different FlexOTO configurations. The contents of the setup file for FlexOTO Hardware Diagram is different that a setup file for FlexOTO Stations. As a result, if you want to save setup information of both the Hardware Diagram and all Test Programs, save a Setup file for FlexOTO Hardware Diagram and a Setup file for each FlexOTO Station.

Screen image files can be saved in many common graphic formats. These screen capture files allow you to document waveforms, results, measurements, and other important displayed items.

Availability of :DISK Commands
SCPI Node FlexOTO
FlexOTO
:DISK:RESults:FNAME ■
:DISK:RESults:FNAME:AUPDate ■
:DISK:RESults:FNAME:USTandard ■
:DISK:RESults:SAVE ■
:DISK:RESults:SAVE:SELection ■
:DISK:SETup:RECall ■ ■
:DISK:SETup:RECall:HCONfig ■ ■
:DISK:SETup:SAVe ■ ■
:DISK:SIMage:CARea ■ ■
:DISK:SIMage:FNAMe ■ ■
:DISK:SIMage:FNAMe:AUPDate ■ ■
:DISK:SIMage:FNAMe:USTandard ■ ■
:DISK:SIMage:IMETadata ■ ■
:DISK:SIMage:INVert ■ ■
:DISK:SIMage:MONochrome ■ ■
:DISK:SIMage:SAVE ■ ■