:TPRogram:REMove:ALL
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:REMove:ALL
This command removes all lines listed for a Station's Test Program. If you want to save the Test Program as a Station Setup file (*.setx) before you clear the Test Program, use the :DISK:SETup:SAVe command. You can recall the Setup file using the :DISK:SETup:RECall command.
Setup files that are saved from FlexOTO Hardware Diagram or a Station are not compatible. A Station Setup file can only be recalled into a Station and a FlexOTO Hardware Diagram Setup file can only be recalled into FlexOTO Hardware Diagram.