:SYSTem:EMBedded?

Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Query Syntax

:SYSTem:EMBedded?

Description

This query returns a "1" (true) if FlexOTO is running embedded on an DCA-X or returns a "0" (false) if it is running on a PC.