:SYSTem:UTCNow?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:SYSTem:UTCNow?
Description
Queries the Coordinated Universal Time (UTC) which was formerly GMT. The time is returned as a string with in the form of <month>/<day>/<year> <hour>:<minutes>:<seconds>. For example,
"12/10/2015 15:47:17"
which represents the 10th day of December 2015, with a time of 15th hour, 47 minutes, and 17 seconds.
Requires FlexOTO revision A.07.00 and above.