:SYSTem:HELP:HEADers?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
:SYSTem:HELP:HEADers?
Description
Returns a ASCII string of all FlexOTO programming commands and queries. Each line lists a command or query followed by a carriage return and line feed. If a command does not support a query, the line is ended with the "/nquery/" characters. If command only supports a query, the line is ended with the "/qonly/" characters. The first line of the returned data is the standard SCPI header for blocks of data. It specifies the data format and how much data will follow.