:SYSTem:FACTory
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:SYSTem:FACTory
Description
Sets FlexOTO to its factory preset settings. Use the *OPC? query to notify the calling program when an operation is complete. Factory preset is the combination of the default settings and additional settings. There is no query form of this command or ability to undo its action.
Use of an *OPC? query to pause program execution while waiting for this command to execute.