:SYSTem:LAUNch

Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Command Syntax

:SYSTem:LAUNch <string>

<string> is the name of an installed DCA-X compliance application.

Description

Launches a DCA-X compliance application, such as the N1012A OIF CEI 3.0 application. Installed applicatons appear on the Apps > Automated Test Apps menu. To determine the proper string, perform the following steps:

  1. Click Tools > SCPI Programming Tools > SCPI Recorder to turn on the SCPI recorder.
  2. Click the Record button.
  3. Click Apps > Automated Test Apps following by the application that you want to launch.
  4. The recorder shows the :LAUNch command with the correct string.

Requires FlexOTO revision A.02.00 and above.

Example Command Sequence

:SYSTem:LAUNch "N1012A OIF CEI 3_0"