:DISPlay Subsystem
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Use the :DISPlay subsystem to configure the jitter transfer swept measurement's Start Frequency, Stop Frequency, Center Frequency, and Stop Frequency and to set the JTF graph's vertical scaling. To set the number of points plotted in the graph, use the :ACQuire subsystem's :ACQuire:FREQuency:PPDecade command. To configure averaging, use the :ACQuire subsystem's :ACQuire:AVERaging and :ACQuire:AVERaging:COUNT commands.