:RESPonse:DISPlay
Flex Apps:
FlexPLL
Command Syntax
:RESPonse{1}:DISPlay {ON | OFF}
Where the {1} character identifies the only available response plots. Because there is only one set of Response plots, this character is optional.
Query Syntax
:RESPonse{1}:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the Response measurements and plots on the JTF graph on or off. If this command is OFF, the state of the :RESPonse:DISPlay:MODel:JTF, :RESPonse:DISPlay:MODel:OJTF, and :RESPonse:DISPlay:MODel:MEASure child commands will have no effect.
Example Command
:RESPonse1:DISPLay ON