Location of Files
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
The Location of FlexPLL User Files picture in this topic shows the FlexPLL folder (with subfolders) for saving files from either a dialog or over SCPI. These folders are the default location for saving specific types of files. For example, screen capture files that you save are, by default, saved in the \Screen Images subfolder. You can always save files to any folder that you wish including those on a network or external drive.
To protect you user files, it is recommended that you backup this folder to an external or network drive.
| Subfolder | Contents | Remote Commands |
|---|---|---|
| Documentation Results | Saved Documentation Wizard report files (.zip). Documentation files can be configured and saved from the GUI. Remotely, they can be configured but not saved. | :DISK:DWIZard:FNAMe |
| Presets | Saved mini-setup files of the following types. Presets can only be saved from dialogs and not programmatically. | |
| CDR Presets. Saved from the Receiver tab of the System Setup dialog. | :CRECovery:PRESets | |
| Source Presets. Saved from the Source tab of the System Setup dialog. | :CRECovery:PRESets | |
| System Presets | :CRECovery:PRESets | |
| Response Calibration | Saved jitter transfer function response calibrations (.jtfx) that is automatically saved during a response calibrations and can be loaded back into FlexPLL. | :CALibrate:RESPonse:STARt |
| Responses | Saved response waveforms (.rspx) that can be loaded and saved | :DISK:RESPonse:SAVE |
| SCPI Scripts | Saved recorded SCPI scripts (.scpi) that can be loaded and saved | :SYSTem:MPButton:FUNCtion |
| Screen Images |
|
:DISK:SIMage:SAVE |
| Setups |
|
:DISK:SETup:SAVE
:DISK:SETup:RECall |