ISerial::ClearToSendState
Description
Shows the current state of the Clear To Send (CTS) input signal.
VB Prototype
Dim value As LineState
                                            value = object.ClearToSendState
                                        
C++ Prototype
HRESULT get_ClearToSendState(
                                        
  LineState* ClearToSendState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview