ISerial::Parity
Description
The parity used with every frame transmitted and received. ASRL_PAR_MARK means that the parity bit exists and is always 1. ASRL_PAR_SPACE means that the parity bit exists and is always 0.
VB Prototype
Dim value As SerialParity
                                            value = object.Parity
                                        
object.Parity = value 
                                        
C++ Prototype
HRESULT get_Parity(
                                        
  SerialParity* Parity
);
		
HRESULT put_Parity(
                                        
  SerialParity Parity
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview