ISerial::DataTerminalReadyState
Description
Manually asserts or deasserts the Data Terminal Ready (DTR) output signal.
VB Prototype
Dim value As LineState
                                            value = object.DataTerminalReadyState
                                        
object.DataTerminalReadyState = value 
                                        
C++ Prototype
HRESULT get_DataTerminalReadyState(
                                        
  LineState* DataTerminalReadyState
);
		
HRESULT put_DataTerminalReadyState(
                                        
  LineState DataTerminalReadyState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview