ISerial::RingIndicatorState
Description
Shows the current state of the Ring Indicator (RI) input signal. The RI signal is often used by modems to indicate that the telephone line is ringing.
VB Prototype
Dim value As LineState
value = object.RingIndicatorState
C++ Prototype
HRESULT get_RingIndicatorState(
LineState* RingIndicatorState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview