ISerial::RequestToSendState
Description
Manually asserts or deasserts the Request To Send (RTS) output signal. When the ASRL_FLOW_CNTRL attribute is set to ASRL_FLOW_RTS_CTS, this attribute is ignored when changed, but can be read to determine whether the background flow control is asserting or unasserting the signal.
VB Prototype
Dim value As LineState
                                            value = object.RequestToSendState
                                        
object.RequestToSendState = value 
                                        
C++ Prototype
HRESULT get_RequestToSendState(
                                        
  LineState* RequestToSendState
);
		
HRESULT put_RequestToSendState(
                                        
  LineState RequestToSendState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview