ISerial::StopBits

Description

The number of stop bits used to indicate the end of a frame.  The value ASRL_STOP_ONE5 indicates one and one-half (1.5) stop bits.

VB Prototype

Dim value As SerialStopBits
value = object.StopBits

object.StopBits = value

C++ Prototype

HRESULT get_StopBits(
  SerialStopBits* StopBits
);

HRESULT put_StopBits(
  SerialStopBits StopBits
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview